Is there a 2-channel version of SN74CBTLV3257RSVR? tried messing around with the name to no avail. figured someone here could find out faster.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a 2-channel version of SN74CBTLV3257RSVR? tried messing around with the name to no avail. figured someone here could find out faster.
Hi Brendan,
Which parameters/features of the SN74CBTLV3257 are most important to you? At a glance the TS5A23159 is a good choice if 105MHz bandwidth is enough.
Here's a list of devices filtered down on the UQFN package, 2 channel 2:1 and powered off protection. If any of these features are negotiable then that opens up our options.
I look forward to hearing back from you!
Thanks!
Alex