hi,
Fout2 inputs a frequency square wave from 10KHZ to 100KHZ, and SEL1 and SEL2 are both high or low levels. SEL3 and SEL4, due to the connection of inverters, have opposite levels to SEL1 and SEL2. When SEL1 and SEL2 are high, 3.3V is used to charge the C31 capacitor and collect current through U14B (TL072CDR) integration. C31 is a capacitive pressure sensor, which is now simulated with a 1pf capacitor. The frequency change output sampling should have changed, but there is no change now. Please help analyze the reason. The schematic diagram is shown below;
Thanks!