Tool/software:
Hi Greetings!
We use TMUX4157N IC.
At S1, GND(ground) is connected, for logic 0.
At S2, NC (no connection), for logic 1.
I expect, the output line be grounded for logic 0
and the output line be OPEN for logic 1, as S2 is NC.
But I observe 0v at the output when Logic is 0.
But 1.16V at the output, when Logic 1 is given, which is not expected. NC
Why is it giving 1.16V?
Thanks in advance.
Thanks & Regards,
Indira