Hi all,
For using load switch(like TPS22920, TPS2292c) for smartphone antenna, I would like to connect Vout to GND.
Then, input is RF from antenna, what capacitor do I have to use?
Antenna signal's bandwidth is 200MHz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
For using load switch(like TPS22920, TPS2292c) for smartphone antenna, I would like to connect Vout to GND.
Then, input is RF from antenna, what capacitor do I have to use?
Antenna signal's bandwidth is 200MHz.
David,
This part is not supported in this sub-fourm this is for the TI signal switch catalog. I would recommend posting in the load switches fourm and see if they can get you the BW for the switch or perhaps they have run RF testing on this part themselves or can recommend a part that supports RF BW signals.
Regards,
Eric N