Hi Team,
May I know if BQ24392 is able to be used in a tablet which support OTG?
Will BQ24392 D+/D- be connected when OTG device plugged in?
My understanding would be since BQ24392 only disconnect D+/D- when DCP or other adapter detected, an OTG as device or host plugged in can still function correctly, just need to add circuit to have tablet generate VBUS(to connector and also to BQ24392 VBUS pin) when opearated as host(Of course they need to design the ID pin detection to act as host or device)
So I think BQ24392 could be used in OTG sytem, is my understanding correct?