Hello,
I am using the TS5A22362 for switching audio audio from a Tablet to an Audio Amplifier or to a 3.5mm Plug.
Since the 3.5mm plug has 4 signals, I'm using two TSA22362 for switching the four signals.
The 3.5mm Plug signals are connected to the NO pins. and the Audio Amplifier is connected to the NC pins
The problem is, when I toggle the IN control signal from the NO to the NC pins, because it makes the change, but when playing music from the Tablet (COM), I can still hear the sound on the NO (that is not longer connected), it hears lower, but I can hear it.
Can you help me, please?