This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it correct to use the body diode on the FET when the device in the OTG mode? Is load switch open in the OTG? Or I need to use additional FET for this purpose?
Vlad,
The load switch will conduct any time there is a voltage present on VBUS >3.6 V.
For example if, let us say the TSU6721 device was on a cell phone and it was OTG mode where the phone is now the host. The phones power management IC (PMIC) would provide the USB standard 5V on the OUT pin of the TSU6721. In the diagram above you can see there is body diode that will conduct in this situation and ~5V - 0.7 V (diode) 4.3 V would appear on VBUS turning on the load switch providing a low impedance path from OUT to VBUS of the TSU6721.
Here is an appnote that explains a little bit more detail of the TSU6721 Accessory and Charger Detection Flow for some extra color beyond the datasheet.
Thank you,
Adam