Hello,
Regarding to input(S1A,S2A) on TS5V330C, my customer is asking a question.
(Question)
・How much voltages is minimum value on input(S1A,S2A) as ABSOLUTE MAXIMUM RATINGS?
From the output voltage range(Vi/o) in datasheet(page4), it becomes to -0.5V.
However the input and output voltage ratings may be exceeded if the input and output clamp-current ratings are observed.
My understanding is correct?
(Generally, the sync level is -300mV on Luma, composite and RGB video signal.)
I’m asking just in case.
Regards,
Tao2199