This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hideto,
We do not currently have data for those specific conditions, but the general trend in the above posted test conditions is that VIH is roughly 70% of VDD and VIL is 30% of VDD when VEE is set to ground. When VEE is -9V and VDD is 9V, we still expect VIH to be about 70% of VDD and VIL to be 30% of VIL. So VIH should be around 6.3V and VIL will be around 2.7V.