This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'd like to know if we have a solution like TS12A12511 only with four channels (dual channels would be also acceptable)
The requirement is to work with negative signaling between -6V and 12 voltages
I would appreciate a quick response, thank you in advance.
Best regards,
Shai Berman
Hi Shai,
What is the needed VCC that this switch can operate with? Do you have dual supply capability?
There is not a 4-channel version of this device. However, we do have a 3-channel SPDT device in the CD4053B which can operate from -6V to 12V input. The Ron of this device is higher but that may not be an issue for your application.