This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm kind of new in this forum, so I'll try to explain my trouble as simple and clear as I can :), if it's not just let me know !
So first of all, the aim of our project is to read a thermistor and connect this termistor to an heating controller. We also want control this heating controller with a digital potentiometer.
To do the job we're using two TS3A24159.
When the thermistor is directly connect to the heating controller everything is ok, the signal is a simple DC signal depending of the thermistor.
But when the signal is going through the both TS3A24159, we have a kind of ripple. And so on the average signal is not the same and when the heating controller read the temperature this is not the same.
Can you please help with some thoughts to rectify this issue. Thanks in advance for your help and support.
Anthony
TSA3A24159.zip
Anthony,
I haven't heard from you so I will close this thread. If you have additional questions responding to this thread will reopen it or you may post a new thread.
thank you,
Adam