Other Parts Discussed in Thread: CD4053B-Q1
Hi Sir,
Could you please help to suggest if you have any CAN BUS MUX are suitable for below application?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CD4053B-Q1
Hi Sir,
Could you please help to suggest if you have any CAN BUS MUX are suitable for below application?
Thank you
Anne,
In the diagram it is difficult to tell how many data lanes and configuration you would like to switch so I will give my interpretation to the diagram below:
Bottom Mux need is a 1-channel 2:1 mux that will take 1 bit from CAN1 and 1 bit from J1708 XCVR and chose which one is selected to connect to the DB15connector.
Middle Mux need is a 1-channel 1:1 mux that will isolate 1 bit from the CAN1 XCVR from the DB15 Connector
Top Mux need is 1-channel 1:1 mux that will isolate 1 bit
Can you confirm the voltage and datarates you would like to support?
CAN1 XCVR
Voltage = 12V
Data rate = 5Mbps
J1708 XCVR
Voltage = 12 V
Data rate = 10 kbps
TI.com switch selection tool has many parts that will support 5Mbps devices but not many that support 12V. If you can use low voltages there are many more options available.
What do you think about the CD4053B-Q1 or TMUX1511device?
Thank you,
Adam