Part Number: SN74LV4052A-Q1
Other Parts Discussed in Thread: SN74HC4852-Q1, SN74HC4852, TS3A5017-Q1
Hello team, I am trying to sense 4-phase current and 4 number of inductor current by using SN74LV4052A-Q1 as below in datasheet.
However I worries about signal distortion in case they add RC filter on the input/output side because MUX R_ds_on is big (100 ohm).
Could you give me the following information? I couldn't find these in the datasheet.
1. Internal model inside the device
2. Resistance range when they add RC filter input and output of the device (I think there is not tight resistance range)
3. Output pin maximum current
4. How output pin is connected with VCC (=internal structure on the output side)
Regards,
Oliver Kim