Other Parts Discussed in Thread: SN74CBT3251, , TMUX1108
I'm looking for a drop-in replacement of TS5N118DBQR. I need nearly the full rail-to-rail range, so the SN74CBT3251 which chops off part of the signal on one side will not work (probably due to being NFET pass transistors with no bootstrapping). TS5N118DBQR seems like a great replacement, but it isn't available from basically anywhere (I assume it was replaced?)
What is the part number for the drop-in replacement for the TS5N118DBQR?
Usage Needed Specs:
Supply: -2.5V to 2.5V
Analog Input: -2.4 to 2.4
On resistance doesn't matter much as long as it is small, the existing design has buffers in-place that can compensate for a wide range of resistances.