This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Arthur,
We are looking for a low current (~10mA) signal mux only. We shall need to switch between two negative input voltages, so a dual supply mux is needed. Output load may be max upto 1nF.
Regards
Gaurav
Hi Adam,
This has an ON resistance of 120 ohm which I think is very high to achieve the desired rise and fall at the output. Please comment!.
Else, if you could provide the spice file, we can simulate in TINA and check.
Regards
Gaurav
Gaurav,
What is your desired on-state resistance? The TMUX1109 device has lower on-state resistance.
Unfortunately we don't have a SPICE model available for the TMUX6119 device.
Thank you,
Adam