This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBT3257: 10MHz Clock input

Part Number: SN74CBT3257
Other Parts Discussed in Thread: TMUX1574

Dear Team,

My customer is looking for 4 channel Single-Pole Double-Throw device.

They will have 10MHz input signal.

Can SN74CBT3257 support this kind of signal?

Which kind of spec. I need to check?

Is there better solution I should promote to the customer?

BR

Kevin