Other Parts Discussed in Thread: SN74CB3T3125,
E2E,
Would sn74cb3t3125 be a higher current allowance to sn74cb3q3125 ? What is the difference between the two?
Thank you,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
E2E,
Would sn74cb3t3125 be a higher current allowance to sn74cb3q3125 ? What is the difference between the two?
Thank you,
Adam
Hi Adam,
The SN74CB3T3125 can support higher current through the switch (±128mA) vs the SN74CB3Q3125 which can support ±64mA.
However, please note that the SN74CB3T devices are a level translation families of switches and multiplexers and do not always pass the signal directly to the output. What is the application you are using the device for?
If you would like to have the signal path pass signals up to 5.5V and have no level translation - I would recommend the SN74CB3Q3125
Here is a link to another E2E post calling out the differences between these device families.