Other Parts Discussed in Thread: SN74CB3Q3257, TMUX1574
Hi,
I'm planning to use TS3L110 to switch 100M Ethernet RX/TX signals between two Ethernet ports. I use the Phy chip LAN8710A and the schematics of this part is shown as attached.
I have following questions:
1. Is the usage of TS3L110 in this schematics correct? (put it directly on the TX/RX differential pairs of the Ethernet signals, before they go into the Ethernet transformer)
2. Is it possible to use SN74CB3Q3257 as a pin-to-pin compatible replacement to TS3L110? from electrical characteristics point of view, I found they are similar,So I'd like to confirm with TI. But there is also some confusing information on the pinout of TS3L110 in the datasheet as mentioned in this question: https://e2e.ti.com/support/switches-multiplexers/f/388/p/828253/3070181#3070181
Thanks for the help!
Regards,
Shan