Part Number: TMUX1247
My question is on the voltage tolerance for the non-selected input. If the switch is say S1 is connected to D, then can the other input, S2 tolerate a higher voltage than the Vdd+0.5 which is called out in the datasheet? As long as S2 is not selected, can it handle 9V?
Thanks, Chip