This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A22362: Stencil for this part?

Part Number: TS5A22362

Hi,

I'm writing to ask if there is a stencil for the part TS5A22362YZPR? Or is there a desktop stencil machine that can make a stencil for the PCB containing this part?

Thank you very much for your help.

Yixin Ma

  • Hi Yixin,

    Great to see that you are trying out the TS5A22362. You can find the example stencil here. This document is located in the product folder for this device, in the "Order Now" tab under the Package/Pins column.

    Let me know if this helps!

    Regards,
    Kate

  • Hi Kate,

    Yes. I decided to use this part because I think the feature of bi-directional current suits the application best. Although the load switch can handle more current, I was having a hard time finding a way to make Vin always positive referenced to the ground. Thank you all for the help in searching the part. I appreciate it very much.

    I still have two questions that might need your help again:

    (1) Any voltage regulator that can help regulate the Vin/Vout to be within -2.5V to 2.5V in the case of voltage spike? The two ends of the power supply meet this criterion in most cases. However, I'll be using this part in an MRI system, the fast-changing magnetic field might cause some voltage fluctuation, so I want to make sure there is enough protection for the part.

    (2) Any microcontrollers from TI that has at least 3 GPIO output pins (can be set to 2.75V) to enable switches on?

    Best regards,

    Yixin

  • Yixin,

    Thanks for your interest in additional TI parts for your system! I recommend asking these questions separately as new posts to the E2E forum to ensure they get to the best team to help you, as I support analog switches & muxes. Feel free to link your previous E2E posts in the new questions to add context, as needed.

    Best regards,
    Kate