Hello,
Is there a alternative to TS3A3166 analog switch which can be used for automotive application? Is it recommended to use in CAN-FD upto 2Mbps for in-vehicle-communication?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is there a alternative to TS3A3166 analog switch which can be used for automotive application? Is it recommended to use in CAN-FD upto 2Mbps for in-vehicle-communication?
Hello Clemens,
Thank you so much for the feedback. COuld you please suggest one switch for CAN-FD 2Mbps application for in-vehicle communication?
What application? What exactly do you want to switch? What voltages are possible?
Hello Clemens,
Switchable termination for CAN-FD bus with 2Mbps... for 12V passenger car applications.
Hello Clemens,
Voltage levels as per standard ISO 11898-2: Road vehicles-CAN.
Standard CAN-FD bus.
Hello Clemens,
we need solution mentioned in this design reference with automotive qualified part in switchable termination.
The TLX9175J is automotive qualified, but has lousy on-state resistance.
The CD4066B-Q1 can switch ± 10 V (when run with a ± 10 V power supply); its typical Ron might be just small enough.
Hi Lalesa,
Is the switch going to be driven from a 5V or a 12V supply?
If you are driving it with a 5V supply, then the TS5A3166-Q1. will work for your application.
For higher supply, the CD4066B-Q1 Clemen's mentioned would be the available option.
Thanks
Saminah