Hi Team,
As subject , my customer is using this device as solution and ask if this device can used for 3.3V SPI signal ?
Andy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
As subject , my customer is using this device as solution and ask if this device can used for 3.3V SPI signal ?
Andy
Hi Andy,
The SN74CBT3257 can be used for 3.3V SPI signal - however the SN74CBTXXXX family of switches are single N-channel FET switches. This means it will not support voltages up to Vcc on the signal path. As you can see below the transfer function of the input to the output is very linear until the input voltage reaches Vcc - ~1V. At this point the FET is beginning to turn off and will clip voltages above Vcc - ~1V.
If you bias the switch Vcc = 5V you will be able to support 3.3 V signals without issue but 5V signals will be clipped to about 4V..
In similar configuration, the new TMUX1574. can support input signals that can range from 0V to VDD and supports SPI signals in addition to other features (1.8-V compatible control inputs, Fail-safe logic).
Regrads
Saminah
Hi Saminah,
nice to reach out again !
follow up on your feedback , customer using 5V as VCC for SN74CBT3257 in their design , so I think it would work for 3.3V SPI signal.
Andy