Hi Team,
Do we have a device to compete against the QPC6324?
Thanks,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have a device to compete against the QPC6324?
Thanks,
Jared
HI Jared,
The QPC6324 is an RF switch with high bandwidth upto 6GHz.
TI currently doesn't characterize or market it's signal switches as "RF" switches. Typically, the term "RF" switch refers to a device that can handle a large amount of power and is on a GaN or GaAs process. TI's signal switches are on a CMOS process and will not handle the same amount of power most people think of when they use the term "RF" switch.
However, we do have the TMUX136 SPDT high-speed switch that supports low power (<20dBm) high speed (6 GHz) applications.
Thanks
Saminah