This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3251: SN74CBTLV3251 output voltage issue

Part Number: SN74CBTLV3251

Hello,

I'm using the sn74cbtlv3251.

In all unconnected pins (i.e. not selected in S0,S1,S2) I measure a voltage of about 0.6~0.7 volts. In the selected pin i measure 3.3V

Even if oe is high, I see this voltage.

My setup is:

VCC = 3.3V

A = 3.3V.

OE = 0V or 3.3V with 10kohm pullup.

I thought the device put all unconnected pins to high Z.

What is wrong?

Thanks,

Ofer.