Hi TI experts,
I'm trying to some circuit simulation to test the TS5A22362. I have the following questions:
1) Can the hspice model that provided on the website be imported into the Cadence PSPICE simulator? I was not able to do that but would like to ask if I missed something. What software should I use for hspice model?
2) Since I cannot import the hspice model into the Cadence PSPICE, I'm building the PSPICE model on my own. I'm having some trouble understanding the Capacitance measurement on the datasheet Figure 16. Between which two nodes are the capacitance measured? Is this capacitance between node NC/NO/IN to the node IN? I'm interested in the On and Off capacitance between COM and NO, should I just add 70pF and 370pF to get that number?
Thank you for your help in advance.
All the best,
Yixin