If VDD = 5.0 (V) and VSEL = 5.0 (V) are applied to the device, it seems to work properly as a switch with R on = 100 kohm and R off = 2 ohm.
However, it does not work properly with VDD = 3.0 (V) and VSEL = 3.0 (V) on the device.
There seemed to be no problem on the datasheet. I do not know what the problem is...
Wouldn't it be possible to use this device to work properly as a switch with R on = 100 kohm and R off = 2 ohm within 3.0 V?
I can't change the operating voltage, so your help is urgent.
Thank you very much.
Woojoong Kim