Part Number: TS12A4516
Other Parts Discussed in Thread: TMUX1511, SN74CB3Q3306A
Hi Team,
My customer wants a chip to apply in his application. They want to a switch or a solution. Here are his requirements:
1.The output follows the input signal, the normal signal level is either 1.8V or 3.3V.
2.Device power supply can be 3.3V or 1.8V.
3.The input signal frequency can be evaluated at 10Mbps.
4.Input the signal that can withstand the surge voltage, it is best to meet the 30V impact after the surge.
5.If the device is powered by 3.3V or 1.8V, it will not be a problem if the input end is long for 5V DC.