I am using a TS5A23159 Analog Switch and the switch on-voltage at ~ 10uA current is 0.4 volts. Is this expected behavior? Can anything be done to get low on-state voltage under these conditions? The part also seems to be drawing ~ 60 mA from the Vcc pin and this is clearly abnormal.