Hello,
In the data-sheet of TS5A23159, there are three terms for current.
(1) On state switch current = +/- 200mA
(2) On state peak switch current = +/-400mA
(3) Continuous current through VCC (ICC) = 100mA
My understanding is that , when switch is turned ON, it can carry maximum of 200mA in either direction, continuous.
It can also handle peak of 400mA for 1 mili second pulse with < 10% duty cycle.
I am bit confusion with terms ICC which is 100mA. I assume that it has nothing to do with ON state current carrying capacity.
If source and load at both end of switch are able to send and receive 200mA current, continuous, this switch will work for my application.
Correct me if my understanding is wrong.
Regards,
khodidas