Part Number: TS12A12511
Other Parts Discussed in Thread: SN74LVC1G3157
hi dear supporting team,
what's the propagation time of TS12A12511 when operating at 50~70M input? and if operate at 1.8V power supply, what't the logic for digital input? tks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS12A12511
Other Parts Discussed in Thread: SN74LVC1G3157
hi dear supporting team,
what's the propagation time of TS12A12511 when operating at 50~70M input? and if operate at 1.8V power supply, what't the logic for digital input? tks!
Vera,
Passive CMOS FET switches like the TS12A12511 have single digit ns to ps propagation delay. The majority of that delay is due to the length of that path which the signal has to travel from one pin to the other. The longest path in a CMOS FET switch primarily the length of the metal leadframe (pin) and bondwire that attaches to the silicon die. The actual silicon CMOS FET switch drain to source delay isn't significant compared to the delay due to the length of pins and bond wires of the IC.
What type of signal are you passing through the switch that you are concerned about the propagation delay?
How did you come to select the TS12A12511 device when there are lower cost options that specify propagation delay tpd? What do you think about using the SN74LVC1G3157?
Thank you,
Adam
hi Adam,
thank you very much for the detail reply!
it is used for SPI signal switch. customer just choose the one which has AVL code. :) I will also recommend3157 as well. tks!