Hi,
On one our boards, we are using this switch to multiplex a logic signal. I had a question here. Can we float one of the selection pin (S1)?
I do not have the use of lower two channels (1B3 & 1B4), so I am just using S0 to switch between 1A-1B1 & 1A-1B2. I could not find input impedance of selection gates on the datasheet. I know recommendations would be to pull S1 low, but I already have a board which needs a fix. So question is, how much would the input impedance on S1 be, to see if that can be left floating with any degree of confidence?
Thanks,
AQ