This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1237: TMUX1237

Part Number: TMUX1237

Hi Sir,

My customer looking for MUX for 24.576MHz Oscillator signal, split to 2 chips.

Do we have kind of solution?

Thanks, Ian.

  • Hi Ian,

     

    The TMUX1237 can possibly support the application. The channel bandwidth is going to vary with supply voltage, load capacitance, and load resistances. For example, the measured channel bandwidth is 400 MHz with a supply voltage of 5 V, Load Capacitance of 5 pF, and load resistance of 50 Ohms, but lower supply voltages, or higher load capacitances / resistances will degrade your channel bandwidth. If you can share that information of the application I will be able to further help narrow down the correct part for the application.

     

     

    Best Regards,

     

    Parker Dodson

  • Hi Ian,

    We haven't heard from you, I will be closing this thread. Feel free to reach out if you have any questions.

    Best Regards,

    Parker Dodson