Other Parts Discussed in Thread: TMUX1511, TMUX1574,
Hi,
I am looking for a smaller SPI level shift solution. The application include a "motor driver” that communicates with “host controller”. SPI voltage for driver is 3.3V while SPI voltage for host controller is 3.3V or 5V. Since the system power is turned on independently, some protection is required even when host controller is power-on and driver is power-off and vice versa.
I looked at various options and I see that one of the devices SN74CBT3125C can support Powered off protection at 5V I/O Voltage. Both TMUX1511 as well as TMUX1574 can support Powered off up to 3.6V.
Can you guys confirm if CBT3125 is the right part that can support Powered off at 5V?
Thanks
Saminah