Other Parts Discussed in Thread: SN74CBTLV3257, TS3A44159, TS5A3166,
Hi
I would need a 2:1 (SPDT) multiplexer to switch the ISO7816 signal for my application.
Basically I would need 3 channels for signal and one channel for power supply.
The max power is around 25mA.
Is it safe to use [S1A S1B] for Vcc power switch and [S2A S2B], [S3A S3B], [S4A S4B] for the communication signal RST, IO and CLK?
Or it is better to choose SN74CBTLV3257 as the channel max current is documented to be 128mA?
Thanks