Other Parts Discussed in Thread: TMUX1511
Hi,
We have finalized SN74CBTLV3245APWR for using it as switch between Ultrascale Plus FPGA and SPI bootflash.
SPI bootflash supports max clock frequency of 166MHz.
But, we are using this SPI flash clock at 127.5Mhz which will be coming from FPGA.
This flash supports DDR also so the data rate will be 255MHz.
So my question is can we use SN74CBTLV3245APWR for 255MHz data rate?
Thanks,
Lalit