Part Number: MSP432P401R
Other Parts Discussed in Thread: ENERGYTRACE
Tool/software: Code Composer Studio
Hello everyone,
I am having some troubles with Energy Trace+ (XDS110-ADD-ON)
the message I am getting is the following:
CORTEX_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 7.0.188.0)
CORTEX_M4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
This happens in the main Blinky as well as in the project that I am working with.
Without the Extension EnergyTrace works fine
*CCS v 8.0
*Xds110Addon
*MSP432 connected via JTAG to the XDS110 (also powered)