Tool/software: Code Composer Studio
Hello Team,
While installing studio on my machine getting the following error message. Please find the attachment.
Studio version: version 8.2.0.
OS: Windows 7 ultimate, 64 bit.
Steps taken:
1 Disabled Antivirus
2 Running studio with admin privileges.
3 Changed the installation directory and retried installation.
Attached one file describing the step at which error occurs.
!SESSION 2018-11-15 10:20:11.832 ----------------------------------------------- eclipse.buildId=4.7.3.M20180301-0715 java.version=1.8.0_112 java.vendor=Oracle Corporation BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US Framework arguments: -application com.ti.common.core.initialize -ccs.profileTag Installed Code Composer Studio 8.2.0.00007. -ccs.removeP2Repositories C:/Users/GHOST/AppData/Local/Temp/ccs_898222d2-37ec-42a1-7768-f8b3debce7ec/repolist.txt Command-line arguments: -os win32 -ws win32 -arch x86 -application com.ti.common.core.initialize -data C:/Users/GHOST/AppData/Local/Temp/ccs_898222d2-37ec-42a1-7768-f8b3debce7ec/workspace -ccs.profileTag Installed Code Composer Studio 8.2.0.00007. -ccs.removeP2Repositories C:/Users/GHOST/AppData/Local/Temp/ccs_898222d2-37ec-42a1-7768-f8b3debce7ec/repolist.txt !ENTRY com.ti.common.core 4 0 2018-11-15 10:20:19.827 !MESSAGE path=ccs_base/DebugServer !ENTRY com.ti.common.core 4 0 2018-11-15 10:20:19.829 !MESSAGE debugServerDir=D:/installs/ccsv8/ccs_base/DebugServer !ENTRY org.eclipse.osgi 4 0 2018-11-15 10:20:29.531 !MESSAGE Application error !STACK 1 java.lang.UnsatisfiedLinkError: D:\installs\ccsv8\ccs_base\DebugServer\bin\LibraryLoader.dll: Can't find dependent libraries at java.lang.ClassLoader$NativeLibrary.load(Native Method) at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1941) at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1824) at java.lang.Runtime.load0(Runtime.java:809) at java.lang.System.load(System.java:1086) at com.ti.debug.engine.xpcom.Runtime.preXPCOMInit(Runtime.java:163) at com.ti.debug.engine.xpcom.Runtime.startBare(Runtime.java:116) at com.ti.debug.engine.xpcom.Runtime.createComponent(Runtime.java:170) at com.ti.utility.filesystem.DirectoryService.<init>(DirectoryService.java:26) at com.ti.utility.filesystem.DirectoryService.<init>(DirectoryService.java:9) at com.ti.utility.filesystem.DirectoryService$SingletonHolder.<clinit>(DirectoryService.java:44) at com.ti.utility.filesystem.DirectoryService.instance(DirectoryService.java:49) at com.ti.common.core.utils.ds.CoreUtilsProvider.getUserHomeDir(CoreUtilsProvider.java:40) at com.ti.common.core.CoreUtils.getUserHomeDir(CoreUtils.java:135) at com.ti.common.core.internal.ExternalReferenceParser.getUserExtRefDir(ExternalReferenceParser.java:176) at com.ti.common.project.core.internal.resexplorer.ResourceExplorerBreadcrumbFileReader.getBreadcrumbFile(ResourceExplorerBreadcrumbFileReader.java:159) at com.ti.common.project.core.internal.resexplorer.ResourceExplorerBreadcrumbFileReader.isDataStale(ResourceExplorerBreadcrumbFileReader.java:147) at com.ti.common.project.core.internal.resexplorer.ResourceExplorerBreadcrumbFileReader.updateData(ResourceExplorerBreadcrumbFileReader.java:77) at com.ti.common.project.core.internal.resexplorer.ResourceExplorerBreadcrumbFileReader.getProductDiscoveryPath(ResourceExplorerBreadcrumbFileReader.java:50) at com.ti.common.project.core.internal.tools.ADiscoveryManager.toSearchPath(ADiscoveryManager.java:375) at org.eclipse.rtsc.project.core.extdiscovery.ExtensionSiteDiscoveryManager.discoverAndInstallExtensionSites(ExtensionSiteDiscoveryManager.java:201) at org.eclipse.rtsc.project.core.extdiscovery.RTSCHeadlessInitializationParticipant.run(RTSCHeadlessInitializationParticipant.java:54) at com.ti.common.core.internal.headless.Initialize.run(Initialize.java:118) at com.ti.common.core.internal.headless.Initialize.start(Initialize.java:76) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243) at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62) at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43) at java.lang.reflect.Method.invoke(Method.java:498) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:653) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:590) at org.eclipse.equinox.launcher.Main.run(Main.java:1499)
Regards,
Tauseef