Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
I have installed and used the porting utility of the CCS v8 ( Version: 8.3.0.00009) to port a previously created project.
I am suspecting it was built in a Unix based platform.
Upon attempting to build the project after a successful port, I was unable to build it because of a path error:
make clean
Cannot run program "make": Launching failed