Other Parts Discussed in Thread: DRV8837, MSP430G2131,
Tool/software: Code Composer Studio
This project was created using a version of compiler that is not currently installed - 4.0.0 [MSP430]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. DRV8837_Customer_EVM_Rev1 properties Problem
when i installed the ccs4 the msp430g2553 board option is not here actually the older programming code is in msp430g2131 i am tring to write it in msp430g2553 what should i do
even i updated my windows latest version and installed right now ccs7 ia m geting the same error in both the ccs7 and ccs4 version