This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO v9.2.0: Trouble on startup

Other Parts Discussed in Thread: CCSTUDIO

Hi,

I have a similar problem with CCStudio v9.2.0. Installed perfectly, but as soon as I launch it, the workspace doesn't open and there is blank white screen like I have attached below. There is an error message as well. 

Here is the error log:

eclipse.buildId=4.8.0.I20180611-0500
java.version=1.8.0_112
java.vendor=Oracle Corporation
BootLoader constants: OS=macosx, ARCH=x86_64, WS=cocoa, NL=en_US
Framework arguments:  -product com.ti.ccstudio.branding.product -keyring /Users/pvj/.eclipse_keyring -showlocation
Command-line arguments:  -os macosx -ws cocoa -arch x86_64 -product com.ti.ccstudio.branding.product -keyring /Users/pvj/.eclipse_keyring -showlocation

!ENTRY org.eclipse.ui.workbench 4 2 2021-08-27 17:54:12.795
!MESSAGE Problems occurred when invoking code from plug-in: "org.eclipse.ui.workbench".
!STACK 0
java.lang.NullPointerException
        at org.eclipse.swt.widgets.Control.internal_new_GC(Control.java:2178)
        at org.eclipse.swt.graphics.GC.<init>(GC.java:174)
        at org.eclipse.swt.graphics.GC.<init>(GC.java:135)
        at org.eclipse.jface.wizard.ProgressMonitorPart.initialize(ProgressMonitorPart.java:237)
        at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:138)
        at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:103)
        at org.eclipse.ui.splash.BasicSplashHandler$AbsolutePositionProgressMonitorPart.<init>(BasicSplashHandler.java:50)
        at org.eclipse.ui.splash.BasicSplashHandler.getBundleProgressMonitor(BasicSplashHandler.java:138)
        at org.eclipse.ui.splash.BasicSplashHandler.getContent(BasicSplashHandler.java:237)
        at org.eclipse.ui.internal.splash.EclipseSplashHandler.init(EclipseSplashHandler.java:107)
        at org.eclipse.ui.internal.Workbench$2.run(Workbench.java:872)
        at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
        at org.eclipse.ui.internal.Workbench.createSplashWrapper(Workbench.java:887)
        at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:631)
        at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336)
        at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:597)
        at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:148)
        at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
        at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
        at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
        at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
        at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
        at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
        at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
        at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
        at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
        at java.lang.reflect.Method.invoke(Method.java:498)
        at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:656)
        at org.eclipse.equinox.launcher.Main.basicRun(Main.java:592)
        at org.eclipse.equinox.launcher.Main.run(Main.java:1498)

!ENTRY org.eclipse.ui 4 0 2021-08-27 17:54:12.801
!MESSAGE Could not instantiate splash
!STACK 0
java.lang.NullPointerException
        at org.eclipse.swt.widgets.Control.internal_new_GC(Control.java:2178)
        at org.eclipse.swt.graphics.GC.<init>(GC.java:174)
        at org.eclipse.swt.graphics.GC.<init>(GC.java:135)
        at org.eclipse.jface.wizard.ProgressMonitorPart.initialize(ProgressMonitorPart.java:237)
        at org.eclipse.jface.wizard.ProgressMonitorPart.<init>(ProgressMonitorPart.java:138)
".log" 11207L, 855755B

Please help. I am using macOS Big Sur Version: 11.5.2

Thanks,

Prakhar

  • Prakhar,

    CCSv9.2 does not support macOS BigSur.  CCSv10.4 is validated on BigSur but there are some UI issues.  Are you tied to using CCSv9.2.  The best version to use with BigSur will actually be CCSv11 as we have upgraded the Eclipse version used in CCS.  I can provide a link to a beta version of CCSv11 if you want.  Otherwise I would recommend CCSv10.4.

    Regards,

    John