This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to build ARM processor project (HalcoGen drivers) on windows 10 machine

Other Parts Discussed in Thread: RM48L952, HALCOGEN, TEST2

Hi,

We are building RM48L952 ARM processor based project in code composer studio successfully on windows 7 machine. But same project giving errors in HalcoGen drivers on windows 10 platform.

Could you help us please?

Description Resource Path Location Type
#1966 cannot open source file "Std_Types.h": The compiler RTS provides (outdated) AUTOSAR 3.1 header files, causing problems for applications which need a later version of AUTOSAR.  To solve that problem, the compiler RTS AUTOSAR files have been moved to a subdirectory of the include directory.  If you still want to use the old AUTOSAR header files, add ${include}/AUTOSAR31 to your include file search path.  If you want to use a later version of AUTOSAR, you will need to get it from a third party. Device_RM48.c /JunoSerialDisplay_ProductionBoard/Drivers/HalCoGen/source line 58 C/C++ Problem
#1966 cannot open source file "Std_Types.h": The compiler RTS provides (outdated) AUTOSAR 3.1 header files, causing problems for applications which need a later version of AUTOSAR.  To solve that problem, the compiler RTS AUTOSAR files have been moved to a subdirectory of the include directory.  If you still want to use the old AUTOSAR header files, add ${include}/AUTOSAR31 to your include file search path.  If you want to use a later version of AUTOSAR, you will need to get it from a third party. ti_fee.h /JunoSerialDisplay_ProductionBoard/Drivers/HalCoGen/include line 97 C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/Device_RM48.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_cancel.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_cfg.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_eraseimmediateblock.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_format.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_Info.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_ini.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_invalidateblock.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_main.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_read.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_readSync.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_shutdown.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_util.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_writeAsync.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: *** [Drivers/HalCoGen/source/ti_fee_writeSync.obj] Error 1 JunoSerialDisplay_ProductionBoard    C/C++ Problem
gmake: Target 'all' not remade because of errors. JunoSerialDisplay_ProductionBoard    C/C++ Problem
#112-D statement is unreachable Footswitch.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 612 C/C++ Problem
#112-D statement is unreachable mainTests.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseTests line 6709 C/C++ Problem
#176-D expression has no effect General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1550 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_ATTask" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 350 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_ClassDevNotify" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 341 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_DevConn" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 344 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_DevDisconn" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 347 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_RxCmd" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 352 C/C++ Problem
#179-D function "App_USBH_BIOLASE_ANDROID_TxCmd" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 355 C/C++ Problem
#179-D function "OS_BSP_RTICompare0Handler" was declared but never referenced os_bsp.c /JunoSerialDisplay_ProductionBoard/BSP line 236 C/C++ Problem
#179-D variable "App_USBH_BIOLASE_ANDROID_CmdsTaskStk" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 99 C/C++ Problem
#179-D variable "App_USBH_BIOLASE_ANDROID_IsConnSem" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 101 C/C++ Problem
#179-D variable "App_USBH_BIOLASE_ANDROID_Ptr" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 100 C/C++ Problem
#179-D variable "cpu_sr" was declared but never referenced os_bsp.c /JunoSerialDisplay_ProductionBoard/BSP line 131 C/C++ Problem
#179-D variable "err" was declared but never referenced Error_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 355 C/C++ Problem
#179-D variable "err" was declared but never referenced Error_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 387 C/C++ Problem
#179-D variable "err" was declared but never referenced Guard_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 131 C/C++ Problem
#179-D variable "err" was declared but never referenced Ready_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 123 C/C++ Problem
#179-D variable "err" was declared but never referenced Ready_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 213 C/C++ Problem
#179-D variable "err" was declared but never referenced Sleep_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 133 C/C++ Problem
#179-D variable "err" was declared but never referenced Standby_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 256 C/C++ Problem
#179-D variable "err" was declared but never referenced Standby_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 298 C/C++ Problem
#179-D variable "err" was declared but never referenced Standby_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 353 C/C++ Problem
#179-D variable "err" was declared but never referenced app.c /JunoSerialDisplay_ProductionBoard/Application line 313 C/C++ Problem
#179-D variable "err" was declared but never referenced mainTests.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseTests line 3348 C/C++ Problem
#179-D variable "errorFlag" was declared but never referenced biolase_tabletSerial.c /JunoSerialDisplay_ProductionBoard/Application/uCSerialAPP line 262 C/C++ Problem
#179-D variable "fanWatts" was declared but never referenced Guard_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 132 C/C++ Problem
#179-D variable "g_brassReadFlash" was declared but never referenced biolase_tabletSerial.c /JunoSerialDisplay_ProductionBoard/Application/uCSerialAPP line 271 C/C++ Problem
#179-D variable "g_receiveCommand" was declared but never referenced biolase_tabletSerial.c /JunoSerialDisplay_ProductionBoard/Application/uCSerialAPP line 274 C/C++ Problem
#179-D variable "host_err" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 399 C/C++ Problem
#179-D variable "htask" was declared but never referenced app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 400 C/C++ Problem
#179-D variable "i" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2114 C/C++ Problem
#179-D variable "i" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2185 C/C++ Problem
#179-D variable "match_val" was declared but never referenced os_bsp.c /JunoSerialDisplay_ProductionBoard/BSP line 129 C/C++ Problem
#179-D variable "maxX" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#179-D variable "newFileName" was declared but never referenced Biolase_SoftwareUpgrade.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationUtilities line 216 C/C++ Problem
#179-D variable "num" was declared but never referenced Footswitch.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 186 C/C++ Problem
#179-D variable "num" was declared but never referenced MRF24J40_rm48_bsp.c /JunoSerialDisplay_ProductionBoard/BSP/WIRELESS_NETWORKING line 526 C/C++ Problem
#179-D variable "num" was declared but never referenced mainTests.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseTests line 6538 C/C++ Problem
#179-D variable "remainingTime" was declared but never referenced Error_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 515 C/C++ Problem
#179-D variable "result" was declared but never referenced Fiber_Cable.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 225 C/C++ Problem
#179-D variable "rti_clk_freq" was declared but never referenced os_bsp.c /JunoSerialDisplay_ProductionBoard/BSP line 128 C/C++ Problem
#179-D variable "steps" was declared but never referenced YSGG.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 323 C/C++ Problem
#179-D variable "stepsTotal" was declared but never referenced YSGG.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 324 C/C++ Problem
#179-D variable "sumNum" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#179-D variable "tableNum" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#179-D variable "test1" was declared but never referenced Firing_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 439 C/C++ Problem
#179-D variable "test2" was declared but never referenced Firing_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 439 C/C++ Problem
#179-D variable "test3" was declared but never referenced Firing_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 439 C/C++ Problem
#179-D variable "testnum" was declared but never referenced Firing_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 438 C/C++ Problem
#179-D variable "testRead" was declared but never referenced sdcard_logging.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseSDCARDLogging line 1896 C/C++ Problem
#179-D variable "totalNum" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#179-D variable "xNum" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#179-D variable "yNum" was declared but never referenced General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 2737 C/C++ Problem
#190-D enumerated type mixed with another type General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1480 C/C++ Problem
#190-D enumerated type mixed with another type General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1489 C/C++ Problem
#190-D enumerated type mixed with another type General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1500 C/C++ Problem
#190-D enumerated type mixed with another type General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1503 C/C++ Problem
#190-D enumerated type mixed with another type Status_Sensor_Pins.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 93 C/C++ Problem
#190-D enumerated type mixed with another type mainTests.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseTests line 3689 C/C++ Problem
#303-D typedef name has already been declared (with same type) os.h /JunoSerialDisplay_ProductionBoard/uCOS/uCOS-II/Source line 29 C/C++ Problem
#551-D variable "p_info" is used before its value is set sdcard_logging.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseSDCARDLogging line 414 C/C++ Problem
#552-D variable "App_USBH_BIOLASE_TABLET_Ptr" was set but never used app_usbh_biolase_tablet.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 74 C/C++ Problem
#552-D variable "edgeCounterValue" was set but never used notification.c /JunoSerialDisplay_ProductionBoard/Drivers/HalCoGen/source line 591 C/C++ Problem
#552-D variable "g_UIC_OAConnectionStatus" was set but never used app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 103 C/C++ Problem
#552-D variable "g_UICConnectionStatus" was set but never used app_usbh_biolase_android.c /JunoSerialDisplay_ProductionBoard/Application/uCUSBAPP/BIOLASE line 102 C/C++ Problem
#552-D variable "oReturnCheck" was set but never used General_Sensor_Calibration.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine/BiolaseApplicationSensorMGMT line 1277 C/C++ Problem
#552-D variable "oReturnCheck" was set but never used biolase_tabletSerial.c /JunoSerialDisplay_ProductionBoard/Application/uCSerialAPP line 1561 C/C++ Problem
#552-D variable "result" was set but never used Standby_State.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseFinalStateMachine line 255 C/C++ Problem
#552-D variable "ui32RcvDat" was set but never used ffBiolase.c /JunoSerialDisplay_ProductionBoard/Drivers/Biolase/source/fat line 105 C/C++ Problem
#552-D variable "x" was set but never used sdcard_logging.c /JunoSerialDisplay_ProductionBoard/Application/BiolaseSDCARDLogging line 1895 C/C++ Problem
Invalid project path: Include path not found (JunoSerialDisplay_ProductionBoard\BSP\IO_EXPANDER). JunoSerialDisplay_ProductionBoard  pathentry Path Entry Problem
This project was created using a version of compiler that is not currently installed - 5.1.6 [Arm]. Another version of the compiler will be used during build - 20.2.5.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. JunoSerialDisplay_ProductionBoard  properties Problem

  • This likely is not related to Windows 7 vs Windows 10.  Based on the last message displayed I suspect that different versions of the Arm compiler are being used.  That last message indicates that the project was set to use the very old 5.1.6 compiler but the version that CCS is using is 20.2.5.LTS.

    When you build on the Windows 7 machine which compiler is it using?

    Regards,

    John