This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Problem: Two developers get binary same .out files upon building the project, a third developer gets a different .out file (it is smaller). But all are using the same CCS version, packages, compiler version etc.
CCS Version: 12.8.1
MSPM0 SDK Version: 2.1.0.03.
Compiler: GNU 9.2.1 (FSF)
Myself and Developer2 get binary same .out files but Developer3 gets a different .out. In looking further into differences, Developer3's CCS seems to generate a different Makefile, how/why can that be given that we are all importing the same CCS project from our code's Git repo and are using the same CCS version etc? Obviously there is something different, but I have now spent a long time with Developer3 going over their system trying to determine any differences. The only thing that stands out to me is that Developer3's CCS install directory is C:\ti\ccs1281 and his his GCC 9.2.1 is in a different directory where as Dev2 and myself have C:\ti\ccs1280. However, we are all confirmed to be using CCS v12.8.1.
I have asked Developer3 to zip his entire project up for me to diff with my local directory and only file differences are:
release.out
release.map
makefile
subdir_rules.mk
See below for the actual file diffs. Every source file and .project, .cproject, and .ccsproject are identical. So how/why is his CCS generating a different makefile?!
file_diffs.zip
Thank you for any assistance!
Hello,
I have asked Developer3 to zip his entire project up for me to diff with my local directory and only file differences are:
release.out
release.map
makefile
subdir_rules.mk
See below for the actual file diffs. Every source file and .project, .cproject, and .ccsproject are identical. So how/why is his CCS generating a different makefile?!
All those files you mentioned can also have information specific to the developer's local environment. Such information includes file path information for source and various utilities, workspace location, timestamps, etc. So unless everyone's PC has everything installed in the same exact directories and are using the same username and build at the same exact time, some differences are expected. The files mentioned are all generated files from the build. These files are typically not in version control.
Every source file and .project, .cproject, and .ccsproject are identical.
These files are expected to be persistent. It is these files that should be checked into version control:
https://dev.ti.com/tirex/explore/node?node=A__AFwtNnyed7LJCr63zDn5xw__ccs_devtools__FUz-xrs__LATEST
Thanks
ki
Thank you for the response, Ki. However, the only item recommended by TI to include in the code repository which I was not, is the .settings directory. I added that and requested Developer3 re-clone and build the project, and the results are identical to last time. Are you saying the .out file will be unique to the environment? If that is the case, how can on ever confirm that two build systems are compiling to the same result? I've added a post-build script to convert the .out to a .bin and those are indeed different between systems still as well.
Are you saying the .out file will be unique to the environment?
It certainly can be. The .out file is a combination of the target code binary that is loaded on the target and also debug symbols used by the debugger for source level debug visibility that is loaded to the CCS debugger on the host PC. It is the latter that has various information that can vary depending on the environment it was built on since it has path information to source files that the debugger needs to find the source files when debugging in CCS.
If that is the case, how can on ever confirm that two build systems are compiling to the same result?
Please see this article: https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/682645/compiler-tms570lc4357-best-practices-for-repeatable-binary-hex-builds
Got it, so it is impossible to ensure build outputs are identical on TI products. There is a chance they can be generated to be the same, which likely involves using he same folder structure for everything involved, but even then there is no guarantee.
Hi,
I invested also quite some time into that kind of an issue: You may have a look here: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1095390/tda4vm-absolute-path-built-in-rodata-section-of-ti-kernel-freertos-components/4132380?tisearch=e2e-sitesearch&keymatch=%252520user%25253A351163#4132380
CCS for me turned out to behave questionable, regarding changing settings regarding how a project has to be build. (compiler, linker settings). Sometimes it does not save the changed options which I made in the settings, sometimes only partly.
Overall, I turned away to use CCS as development tool, I only use it to debug my projects. The projects are built now by cmake, which configuration is transparent and checked into git repos. So no more issues that build options can vary between CCS instances. (Hint: I assume CCS also just use cmake to generate makefiles to build the project internally.)
Despite of all that, you have to be aware, that in some libs from TI are C macros used, which embeddeds information of the building machine in your binary. (__FILE__)
Regards,
Thomas
Overall, I turned away to use CCS as development tool, I only use it to debug my projects. The projects are built now by cmake, which configuration is transparent and checked into git repos. So no more issues that build options can vary between CCS instances. (Hint: I assume CCS also just use cmake to generate makefiles to build the project internally.)
Sorry to hear of your frustrations using CCS as a build environment. cmake is a popular environment and there are many who use it to build outside the CCS environment and just use CCS to debug like you are planning.
CCS does not use cmake under the hood. CDT is used to generate makefiles from the project and then gmake is called:
Thank you Thomas. I may very well go down that path too and your information will be most helpful!