This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My colleague just installed CCS4 but none of the projects build with his installation. I noticed that the system variable ProjDirPath was defined incorrectly. How does this get defined in the first place so that we can correct it? The project was imported and everything works correctly on my machine. We each define a custom macro for our top directory from which all succeeding directories are identical. This macro is defined in window->preferences->General->Workspace->linked resources and is correctly used. But the ProjDirPath points to the wrong directory. There are several other users and we can all build this project fine so there's nothing wrong with the project, the problem must lie in the setup or import of the project or the CCS installation. Any ideas?
Since the path for ProjDirPath is incorrect and many paths are based on this, the compiler cannot find the include files it needs to build the project. I understand it is a system variable that cannot be changed but it gets set somehow so how is it done in the first place. How does the "system" know what to set it to?
It sets it to location of project files (i.e. .project .cdtbuild). Did you by any chance have "Copy projects into workspace" option enabled? This would physically copy project files into a different location,. thus adjusting its path. However, if your project files are part of a larger source tree that remains in its original location, then that could be one of the reasons whey macro might appear to be invalid.
martin