This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

System macro ProjDirPath defined incorrectly

My colleague just installed CCS4 but none of the projects build with his installation.  I noticed that the system variable ProjDirPath  was defined incorrectly. How does this get defined in the first place so that we can correct it?  The project was imported and everything works correctly on my machine.  We each define a custom macro for our top directory from which all succeeding directories are identical.  This macro is defined in window->preferences->General->Workspace->linked resources and is correctly used. But the ProjDirPath points to the wrong directory.  There are several other users and we can all build this project fine so there's nothing wrong with the project, the problem must lie in the setup or import of the project or the CCS installation.  Any ideas?