This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5: .cproject touched when changing active build configuration

I use CCS5.0.1 plus patch idecore_setup_5.0.2.N201103291000. The problem that .cproject files are touched every time when opening a project is solved with that patch. But the issue still exists when I change the active build configuration.

Would it be possible to correct this behavior as it was done in the patch for the opening procedure?