Part Number: CODECOMPOSER
I'm using KDE Neon dsistribution (Ubuntu 20.04 under the hood). I've downloaded and installed CCS11.1.0.00011_linux-x64.tar.gz. Additionaly I've installed ti-processor-sdk-rtos-am335x-evm-06.03.00.106-Linux-x86-Install.bin. I've generated some example projects in PDK for bbbAM335x and evmAM335x. I've imported a few examples to CC Studio. I'm trying to open application *.cfg with XGCONF (rigth mouse click on te app.cfg, choose Open with and click on XGCONF) and .... nothing happens. CC Studio seems hanging. It looks like:

The only thing I can do is to kill CC Studio process.
I've tried the same thing on Windows version (Win 10 in Virtualbox) and it works properly.
What can I do to get XGCONF working in Linux ?