This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using KDE Neon dsistribution (Ubuntu 20.04 under the hood). I've downloaded and installed CCS11.1.0.00011_linux-x64.tar.gz. Additionaly I've installed ti-processor-sdk-rtos-am335x-evm-06.03.00.106-Linux-x86-Install.bin. I've generated some example projects in PDK for bbbAM335x and evmAM335x. I've imported a few examples to CC Studio. I'm trying to open application *.cfg with XGCONF (rigth mouse click on te app.cfg, choose Open with and click on XGCONF) and .... nothing happens. CC Studio seems hanging. It looks like:
The only thing I can do is to kill CC Studio process.
I've tried the same thing on Windows version (Win 10 in Virtualbox) and it works properly.
What can I do to get XGCONF working in Linux ?
Hi Ki,
I've installed ti-processor-sdk-rtos-am335x-evm-06.03.00.106-Linux-x86-Install.bin - this installs into ~/ti directory:
- bios_6_76_03_01
- pdk_am335x_1_0_17
- processor_sdk_rtos_am335x_6_03_00_106
- xcdtools_3_55_02_22_core
But CC Studio installed its own version of xcdtools into ~/ti/ccs1110 directory: xcdtools_3_62_01_16_core
Thanks. I installed the same versions of BIOS and XDCtools with my CCS 11.1.0 instalaltion on Ubuntu 20.04. When trying to open the cfg file with XGCONF, I initially had the same issue where a blank tab for the cfg file was opened and a small spinning circle doing nothing for awhile. After a long wait of a few minutes, the cfg file opened correctly with valid content.
I assume in your case, the cfg file just remains blank - never displaying content. You mentioned CCS looking like it hanged. Did it actually hang where the entire IDE is not responsive?
Also, please attach your workspace log file. It should be in <WORKSPACE FOLDER>/.metadata/.log
Thanks
ki
Thanks. I installed the same versions of BIOS and XDCtools with my CCS 11.1.0 instalaltion on Ubuntu 20.04. When trying to open the cfg file with XGCONF, I initially had the same issue where a blank tab for the cfg file was opened and a small spinning circle doing nothing for awhile. After a long wait of a few minutes, the cfg file opened correctly with valid content.
I've waited even 15 minutes and I think it is enough time to wait for loading file in XGCONF :)
I assume in your case, the cfg file just remains blank - never displaying content. You mentioned CCS looking like it hanged. Did it actually hang where the entire IDE is not responsive?
It hangs completely, entire IDE is not responsive. I can only kill the process on console or in KDE system monitor.
Also, please attach your workspace log file. It should be in <WORKSPACE FOLDER>/.metadata/.log
OK, here is the log file.
Thanks,
I've waited even 15 minutes and I think it is enough time to wait for loading file in XGCONF :)
Yes, I only wait like 1-2 minutes at most.
Thanks for the log. Can you also share your cfg file?
Thanks
ki
Thanks for the log. Can you also share your cfg file?
Do you mean app cfg file which I try to open in XGCONF? I attach this cfg.
Thanks. I do not see any issue with this particular cfg. Do you have issues will all cfg files with XGCONF? Can you try creating a simple new project using the SYS/BIOS "Typical" project and see if the generated cfg from that project also has the issue?
Thanks
ki
Thanks. I do not see any issue with this particular cfg. Do you have issues will all cfg files with XGCONF? Can you try creating a simple new project using the SYS/BIOS "Typical" project and see if the generated cfg from that project also has the issue?
I've tried few sample projects and also tried to create new projects using SYS/BIOS "Typical" project - unfortunately all of this projects cfg cuases the same issue.
Thank you for trying it out. Perhaps it is specific to KDE Neon. This is not an environment we test on. I will see if I can set up such an environment and try it out.
Thanks
ki
I'm setting up a KDE neon VM right now. It will take some time to configure. Once I have it set up, I'll see if I can reproduce the issue.
I set up a KDE neon 5.24 VM and installed CCS 11.1.0 on it. I am able to open your cfg file in xgconf. Hence it is not a KDE neon issue but something more specific to your local environment.
Have you tried some of the other troubleshooting tips like cleaning your workspace?
I've tested two things before the weekend:
1. Cleaning workspace doesn't change anything.
2. I've installed fresh KDE Neon User iso from the web in Virtualbox. XGCONF works.
And today I've returned after the weekend to this issue. Due the weekend my version of KDE (I've installed it from iso about 3 months ago) get huge update (~220 packets). I've installed this update today morning. And what a surprise ... Now XGCONF works. I've suspected Eclipse which I had installed to build projects for Beaglebone Black, but it turned out that some system packet (library ?) was guilty. I have apt history.log with info what was upgraded, but analysis which packet was ressponsible for this issue is not what I want to do overnight ;)