This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which project files to exclude from version control?

Hi,

I share an msp430 project through subversion with another engineer using CCS 4.2.3.00004.  When I open the project that he's checked in, I get no files listed.  I've tried editing files to change absolute paths to no avail and the only way I was able to get the project to open as expected was to place it in the same directory structure as exists on the other engineer's machine.  We've tried to use linked resources (my kingdom for a symlink!), but haven't gotten that to work just yet.

Is there a subset of files that must be ignored in order for sharing projects across subversion that might help solve this problem, or is there a better way to do this?

 

Thanks!

,

John