In what cases would dbgjtag pass and CCS give the following error when connecting?:
CPU_4: Error connecting to the target: (Error -1052 @ 0xDED3) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Release 5.0.333.0)
dbgjtag passes all of its tests (integrity, givendata, brokenpath, pathlength returns IR=32bits and DR=4bits).
TDI, TDO, TMS, TCLK, TRST all toggle on the board, and the timing looks reasonable. EMU0 and 1 are always high. I have tried clock frequencies of 100kHz, 1MHz, 5MHz, and 10MHz in CCS, and all give the same result. The DSK5416 evaluation board works fine using the same emulator.
Some more details:
CCS version: 4.2.3.00004
DSP: C5441
Emulator: XDS100v2
I would appreciate any ideas.
Thanks,
Chris