This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is anyone using both CCS4 and IAR workbench for development? After using CCS4 for a workbook, returning to IAR I had a problem with the MSP430
FET TOOL. Is there a problem?
Hi Frank,
It is possible to use both tools on PC without problem.
It might be good to have a bit further information in order to help you but there are two things that I would like you to check:
- what MSP are you using? If it is one that supports both JTAG and Spy-bi-wire then in IAR you need to choose this manually. Please make sure this is done in the debug options. It is under Project - options - TI Debugger I believe.
- how old is your IAR installation? If IAR was using an older MSP430 dll and then CCS was installed with a newer version, this tends to cause issues. Ways to get around this are to
1) upgrade IAR
2) manually update the dll file. This can be done by backing up *important* the msp430.dll and hil.dll files in your IAR directories. After backup replace them with the ones from CCS.
Please give the above a check. If it does not solve the issue, please let me know exactly what issue/error you are getting.
Cheers,
Lisa
Hi Frank,
Great, glad to hear that did the trick. All the best with the tools.
Cheers,
Lisa